:RMEMory:PLLModel:ALOop:COPY
Flex Apps:
FlexPLL
Command Syntax
:RMEMory{1:4}:PLLModel:ALOop:COPY
Where the {1:4} specifier identifies one of four possible JTF response memories. For example, :RMEMory3:PLLModel:ALOop:COPY.
Description
Copies FlexPLL's automatically calculated parameters for Response JTF and OJTF models into the following manual loop parameters settings. This provides you convenient starting settings for viewing the effects of adjusting the parameters on the displayed model plots using the following commands:
- Loop Gain (
:RMEMory:PLLModel:MLOop:GAIN) - Loop Pole (
:RMEMory:PLLModel:MLOop:POLE) - Loop Zero (
:RMEMory:PLLModel:MLOop:ZERO)
Example Command
:RMEMory2:PLLModel:ALOop:COPY