:RMEMory:PLLModel:DUT:LORDer
Flex Apps:
FlexPLL
Command Syntax
:RMEMory{1:4}:PLLModel:DUT:LORDer {FIRSt | SECond | THIRd | FOURth}
Where the {1:4} specifier identifies one of four possible JTF response memories. For example, :RMEMory3:PLLModel:DUT:LORDer.
Query Syntax
:RMEMory{1:4}:PLLModel:DUT:LORDer?
Description
Specifies the DUT's PLL order as being First, Second, Third, or Fourth. The loop order that you select is applied to automatically and manually calculated Response memory models.
Example Command
:RMEMory2:PLLModel:DUT:LORDer FIRSt