:RMEMory:UNAMe
Flex Apps:
FlexPLL
Command Syntax
:RMEMory{1:4}:UNAMe "<string>"
Where the {1:4} specifier identifies one of four possible JTF response memories. For example, :RMEMory3:UNAMe.
Query Syntax
:RMEMory{1:4}:UNAMe?
Description
Assigns a custom user name to the response Memory plots on the JTF graph. The default names are "Memory 1", "Memory 2", "Memory 3", and "Memory 4". User names are displayed on the screen and on screen captures. To return a user name to its default value, send an empty string with this command.
The maximum length of the custom name is 255 characters.
Example Command
:RESPonse:UNAMe "DUT 18"