:RMEMory:FILE:NAME
Flex Apps:
FlexPLL
Command Syntax
:RMEMory{1:4}:FILE:NAME <filename>
Where the {1:4} specifier identifies one of four possible JTF response memories. For example, :RMEMory3.
Description
Enters the name (including path) of a Response file that is to be loaded into an Response Memory. Use the :RMEMory:FILE:LOAD command to actually load the file. If no path is given, the file expected to be in the default \Responses user-data folder.
C:\Users\user\Documents\Keysight\FlexPLL>\Responses
Example Command
:RMEMory2:FILE:NAME "test-response"