:RMEMory:SMeasure
Flex Apps:
FlexPLL
Command Syntax
:RMEMory{1:4}:SMeasure {MBANdwidth{1} | MFGain{1} | MFPole{1} | MFTail{1} |
MFZero{1} | MAVerage{1} | MMAXimum{1} | MMINimum{1} | MTAil{1} | MPEaking{1} | MQFactor{1}}
Where the {1:4} specifier identifies one of four possible JTF response memories. For example, :RMEMory3:SMeasure.
Query Syntax
:RMEMory{1:4}:SMeasure?
Description
For the selected response Memory, selects a measurement in the displayed results table. For the Bandwidth and Peaking measurements, this displays annotation on the corresponding location on the displayed plot. For example, to select the Peaking measurement on response memory 2:
:RMEMory2:SMeasure MPEaking2
Selecting a measurement in the table has no effect on the task of returning the selected (or any other) measurement value. For example, you could optionally select the Bandwidth measurement, but return the current Flatness measurement with the :MEASure:RMEMory2:FLATness? query.
| Measurement | Argument | Query Response |
|---|---|---|
| Bandwidth | MBANdwidth{1} | MBAN{1} |
| Peaking | MPEaking{1} | MPE{1} |
| Maximum | MMAXimum{1} | MMA{1} |
| Minimum | MMINimum{1} | MMI{1} |
| Average | MAVerage{1} | MAV{1} |
| fGain | MFGain{1} | MFG{1} |
| fZero | MFZero{1} | MFZ{1} |
| fPole | MFPole{1} | MFP{1} |
| Q Factor | MQFactor{1} | MQF{1} |
| fTail | MFTail{1} | MFT{1} |
| mTail | MMTail{1} | MMT{1} |
Example Command
:RMEMory2:SMeasure MBANdwidth1