:CHANnel:COPY

Command Syntax

:CHANnelN:COPY {CHANnel
                    <source>
                }

Where N identifies a destination channel into which settings are copied. N is in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, CHANnel1_2.

Where <source> identifies a source channel from which to copy settings. <source> is in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, 2B.

Description

Copies channels settings from a source channel into the destination channel. Copied settings include the following:

  • Scale
  • Offset
  • Hardware Skew
  • Software Delay
  • Signal Type Auto Detect and Type
  • External Transducer settings
  • External Attenuator settings

The copied settings do not include waveform color or any custom waveform name.