:CHANnel:CWINdow
Command Syntax
:CHANnelN:CWINdow TIME{1:4}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:CWINdow?
Description
The :CHANnel{N}:CWINdow command allows you to assign a waveform to a Waveform content window.
| Argument | Displayed Waveform Content Window |
Number of Available Windows |
Scale Units | |
|---|---|---|---|---|
| Programmatically | Via Front Panel |
|||
| TIME{1:4} | Waveform | 4 | 4 | Y-Axis: Volts or Watts (linear scale) X-Axis: seconds |