:CHANnel:PATTern:FILE:GCODe

Command Syntax

:CHANnelN:PATTern:FILE:GCODe {ON | OFF | 1 | 0}

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:PATTern:FILE:GCODe?

Query Response

{1 | 0}

Description

When you have specified a PAM4 signal type (see :CHANnel:SIGNal:TYPE), this command lets you specify whether symbols are Gray Coded or uncoded. When patterns are specified (see :CHANnel:PATTern:FILE:NAME), the pattern must match this selection.