:CHANnel:SRANge?

Query Syntax

:CHANnelN:SRANge?

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Description

This query returns the actual available hardware range of the channel based on the total channel gain, channel scale and offset, probe state, and probe offset mode. The lower and upper values of the range are returned comma-separated.