:CHANnel:IMPedance

Command Syntax

:CHANnelN:IMPedance {FIFTy}

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:IMPedance?

Description

If an oscilloscope has options for setting the input channel impedance, this command lets you select from the supported options.

The query returns the type of impedance set for the oscilloscope input channel.