:CHANnel:DISPlay
Command Syntax
:CHANnelN:DISPlay {ON | OFF | 1 | 0}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:DISPlay?
Query Response
{1 | 0}
Description
Turns the display of the specified channel on or off. Use the :CHANnel:STATus? command to determine if a channel is available for display.