:CHANnel:DB?
Query Syntax
:CHANnelN:DB?
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Description
The query returns, as dB, the total attenuation/gain/dB of the channel including all probes, accessories, and external scaling.
You can also return the channel's total attenuation/gain/dB using the :CHANnel:ATTenuation? or :CHANnel:GAIN? commands, respectively. These commands give you three ways of interpreting the same setting.