:CHANnel:PATTern:INVert

Command Syntax

:CHANnelN:PATTern:INVert {{ON | 1} | {OFF | 0}}

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:PATTern:INVert?

Query Response

{1 | 0}

Description

When detecting a known pattern or a pattern that is loaded from a file (see :CHANnel:PATTern:MODE), this command lets you detect an inverted version of the known or loaded pattern.