:CHANnel:PATTern:FILE:RELoad

Command Syntax

:CHANnelN:PATTern:FILE:RELoad

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Description

When you have specified a PAM signal type (see :CHANnel:SIGNal:TYPE) and specified the signal pattern by loading a pattern file (see :CHANnel:PATTern:FILE:NAME), this command reloads the specified pattern file. Reloading is useful when there have been changes to the pattern file that was previously loaded.