:CHANnel:PATTern:FILE:NAME
Command Syntax
:CHANnelN:PATTern:FILE:NAME "filename"
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:PATTern:FILE:NAME?
Query Response
"string"
Description
When you have chosen "loading a pattern file" to identify the data signal pattern (see :CHANnel:PATTern:MODE), this command lets you specify the name of the file to load. The file name is a quoted full-path string.
If there are changes to the pattern file that has been loaded, use the :CHANnel:PATTern:FILE:RELoad command.