:STATus:ADERegister:ENABle

Command Syntax

:STATus:ADERegister:ENABle <mask>

<mask> is an integer, 0 to 255, representing a mask for the bits in the event register.

Query Syntax

:STATus:ADERegister:ENABle?

Description

Enters a decimal-weighted value in the enable register that masks the ability to report bits in the Acquisition Done Register (see :STATus:ADERegister:EVENt?).

Acquisition Done Register Commands
Register Read Write Command
Event ♦   :STATus:ADERegister:EVENt?
Enable (mask) ♦ ♦ :STATus:ADERegister:ENABle
Acquisition Done Register Bits
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32768 16384 8192 4096 2048 1024 512 256 128 64 32 16 8 4 2 1
Event
Register
— — — — — — — — — — — — — — — ADER
Enable
Register
                               
Sets to Bit 0 (ADER) of Operation Status Register

Bit Definitions

ADER
A true indicates that the acquisition has completed and data is ready.