:STATus:OVERload:ALL:CONNection:BANK:EVENt?

Query Syntax

:STATus:OVERload:ALL:CONNectionN:BANKM:EVENt?

Where N identifies one of up to eight {1:8} connections that can be used for instruments.

Where M identifies a bank of up to 8 channels. Current oscilloscopes supported by Infiniium are all less than 8 channels, so M is always "1" (or not used).

Description

Reads the Overload All Connection Bank register to see which channels have reported an overload since the last time the register was read.

Reading the register once will clear the status for all channels.

Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically "OR"ed, which results in setting true bit M-1 (BANKM) of the Overload All Connection Register.

Overload All Connection Bank Register Commands
Register Read Write Command
Event ♦   :STATus:OVERload:ALL:CONNection:BANK:EVENt?
Enable (mask) ♦ ♦ :STATus:OVERload:ALL:CONNection:BANK:ENABle
Overload All Connection Bank Register Bits
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32768 16384 8192 4096 2048 1024 512 256 128 64 32 16 8 4 2 1
Event
Register
— — — — — — — — CH8 CH7 CH6 CH5 CH4 CH3 CH2 CH1
Enable
Register
                               
Sets to Bit M-1 (BANKM) of Overload All Connection Register

Bit Definitions

CH1-CH8
A true indicates the channel has reported an overload since the last time the register was read. If the oscilloscope has fewer than eight channels, only those bits are used.