:STATus:CALibration:EVENt?

Query Syntax

:STATus:CALibration:EVENt?

Description

Reads the calibration event register to determine the status of individual status bits. The decimal-weighted value of the register is returned. The only bit used in this register is bit 0 (DONE), which indicated if a calibration has completed.

Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically "OR"ed, which results in setting true bit 14 (CAL) of the Operation Status Register.

Use the :CALibrate Subsystem subsystem to run a calibration.

Calibration Register Commands
Register Read Write Command
Event ♦   :STATus:CALibration:EVENt?
Enable (mask) ♦ ♦ :STATus:CALibration:ENABle
Calibration Status Register Bits
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32768 16384 8192 4096 2048 1024 512 256 128 64 32 16 8 4 2 1
Event
Register
— — — — — — — — — — — — — — — DONE
Enable
Register
                               
Sets to Bit 14 (CAL) of Operation Status Register

Bit Definitions

DONE
True indicates that a calibration has completed.