:STATus:CLIPped:EVENt?

Query Syntax

:STATus:CLIPped:EVENt?

Description

Reads the Clipped register to see which channels that have reported ADC clipping since the last time the register was read.

Reading the register once will clear the status for all channels.

Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically "OR"ed, which results in setting true bit 7 (CLIP) of the Operation Status Register.

Clipped Register Commands
Register Read Write Command
Event ♦   :STATus:CLIPped:EVENt?
Enable (mask) ♦ ♦ :STATus:CLIPped:ENABle
Clipped Register Bits
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32768 16384 8192 4096 2048 1024 512 256 128 64 32 16 8 4 2 1
Event
Register
— — — — — — — — CH8 CH7 CH6 CH5 CH4 CH3 CH2 CH1
Enable
Register
                               
Sets to Bit 7 (CLIP) of Operation Status Register

When there is only one oscilloscope connection in the system and that oscilloscope has eight or fewer channels (that is, it needs only one bank), the Clipped Registers give you a shortcut to the Clipped All Connection 1 Bank 1 registers which have the same content but ultimately cascade to a different summary bit in the Operation Status Register.

Bit Definitions

CH1-CH8
A true indicates the channel has reported ADC clipping since the last time the register was read. If the oscilloscope has fewer than eight channels, only those bits are used.