:STATus:TRIGger:ENABle

Command Syntax

:STATus:TRIGger:ENABle <mask>

<mask> is an integer, 0 to 65535, representing a mask for the bits in the event register.

Query Syntax

:STATus:TRIGger:ENABle?

Description

Enters a decimal-weighted value in the enable register that masks the ability to report bits in the Trigger Event Register (see :STATus:TRIGger:EVENt?).

Trigger Event Register Commands
Register Read Write Command
Event ♦   :STATus:TRIGger:EVENt?
Enable (mask) ♦ ♦ :STATus:TRIGger:ENABle
Trigger Event Register Bits
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32768 16384 8192 4096 2048 1024 512 256 128 64 32 16 8 4 2 1
Event
Register
— — — — — — — — — — — — — STER ATER AER
Enable
Register
                               
Sets to Bit 5 (AER) of Operation Status Register

Bit Definitions

STER
A true indicates that a software (qualified) trigger has occurred.
ATER
When trigger sweep is set to Auto, a true indicates the wait period for a valid hardware or software (qualified) trigger has elapsed and an auto trigger has occurred.
AER
A true indicates that hardware is armed and ready to trigger.