:STATus:CLIPped:ALL:ENABle

Command Syntax

:STATus:CLIPped:ALL:ENABle <mask>

<mask> is an integer, 0 to 65535, representing a mask for the bits in the event register.

Query Syntax

:STATus:CLIPped:ALL:ENABle?

Description

Enters a decimal-weighted value in the enable register that masks the ability to report bits in the Clipped All Register (see :STATus:CLIPped:ALL:EVENt?).

Clipped All Register Commands
Register Read Write Command
Event ♦   :STATus:CLIPped:ALL:EVENt?
Enable (mask) ♦ ♦ :STATus:CLIPped:ALL:ENABle
Clipped All Register Bits
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32768 16384 8192 4096 2048 1024 512 256 128 64 32 16 8 4 2 1
Event
Register
— — — — — — — — CONN8 CONN7 CONN6 CONN5 CONN4 CONN3 CONN2 CONN1
Enable
Register
                               
Sets to Bit 8 (CLIP-ALL) of Operation Status Register

Bit Definitions

CONN1-CONN8
A true indicates the instrument on the connection has reported ADC clipping since the last time the register was read. If there are fewer than eight instruments/connections, only those bits are used.