:STATus:TRIGger:EVENt?

Query Syntax

:STATus:TRIGger:EVENt?

Description

Reads the Trigger Event Register to determine the status of individual status bits. The decimal-weighted value of the register is returned.

Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically "OR"ed, which results in setting true bit 2 (TRIG) of the Operation Status Register.

Armed Event Register Commands
Register Read Write Command
Event ♦   :STATus:TRIGger:EVENt?
Enable (mask) ♦ ♦ :STATus:TRIGger:ENABle
Armed Event Register Bits
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32768 16384 8192 4096 2048 1024 512 256 128 64 32 16 8 4 2 1
Event
Register
— — — — — — — — — — — — — STER ATER AER
Enable
Register
                               
Sets to Bit 2 (TRIG) of Operation Status Register

Bit Definitions

STER
A true indicates that a software (qualified) trigger has occurred.
ATER
When trigger sweep is set to Auto, a true indicates the wait period for a valid hardware or software (qualified) trigger has elapsed and an auto trigger has occurred.
AER
A true indicates that hardware is armed and ready to trigger.