:STATus:CLIPped:ALL:CONNection:ENABle

Command Syntax

:STATus:CLIPped:ALL:CONNectionN:ENABle <mask>

<mask> is an integer, 0 to 65535, representing a mask for the bits in the event register.

Query Syntax

:STATus:CLIPped:ALL:CONNectionN:ENABle?

Description

Enters a decimal-weighted value in the enable register that masks the ability to report bits in the Clipped All Connection Register (see :STATus:CLIPped:ALL:CONNection:EVENt?).

Clipped All Connection Register Commands
Register Read Write Command
Event ♦   :STATus:CLIPped:ALL:CONNection:EVENt?
Enable (mask) ♦ ♦ :STATus:CLIPped:ALL:CONNection:ENABle
Clipped All Connection Register Bits
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32768 16384 8192 4096 2048 1024 512 256 128 64 32 16 8 4 2 1
Event
Register
— — — — — — — — — — — — — — — BANK1
Enable
Register
                               
Sets to Bit N-1 (CONNN) of Clipped All Register

Bit Definitions

BANK1
A true indicates the channels on bank 1 reported ADC clipping since the last time the register was read.