:STATus:OVERload:ALL:EVENt?

Query Syntax

:STATus:OVERload:ALL:EVENt?

Description

Reads the Overload All register to see which instruments have reported channel overloads since the last time the register was read.

Reading the register once will clear the status for all instruments.

Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically "OR"ed, which results in setting true bit 13 (OVLD-ALL) of the Operation Status Register.

Overload All Register Commands
Register Read Write Command
Event ♦   :STATus:OVERload:ALL:EVENt?
Enable (mask) ♦ ♦ :STATus:OVERload:ALL:ENABle
Overload All Register Bits
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32768 16384 8192 4096 2048 1024 512 256 128 64 32 16 8 4 2 1
Event
Register
— — — — — — — — CONN8 CONN7 CONN6 CONN5 CONN4 CONN3 CONN2 CONN1
Enable
Register
                               
Sets to Bit 13 (OVLD-ALL) of Operation Status Register

Bit Definitions

CONN1-CONN8
A true indicates the instrument on the connection has reported channel overloads since the last time the register was read. If there are fewer than eight instruments/connections, only those bits are used.