:STATus:CLIPped:ALL:CONNection:BANK:ENABle

Command Syntax

:STATus:CLIPped:ALL:CONNectionN:BANKM:ENABle <mask>

Where N identifies one of up to eight {1:8} connections that can be used for instruments.

Where M identifies a bank of up to 8 channels. Current oscilloscopes supported by Infiniium are all less than 8 channels, so M is always "1" (or not used).

<mask> is an integer, 0 to 65535, representing a mask for the bits in the event register.

Query Syntax

:STATus:CLIPped:ALL:CONNectionN:BANKM:ENABle?

Description

Enters a decimal-weighted value in the enable register that masks the ability to report bits in the Clipped All Connection Bank Register (see :STATus:CLIPped:ALL:CONNection:BANK:EVENt?).

Clipped All Connection Bank Register Commands
Register Read Write Command
Event ♦   :STATus:CLIPped:ALL:CONNection:BANK:EVENt?
Enable (mask) ♦ ♦ :STATus:CLIPped:ALL:CONNection:BANK:ENABle
Clipped All Connection Bank Register Bits
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32768 16384 8192 4096 2048 1024 512 256 128 64 32 16 8 4 2 1
Event
Register
— — — — — — — — CH8 CH7 CH6 CH5 CH4 CH3 CH2 CH1
Enable
Register
                               
Sets to Bit M-1 (BANKM) of Clipped All Connection Register

Bit Definitions

CH1-CH8
A true indicates the channel has reported ADC clipping since the last time the register was read. If the oscilloscope has fewer than eight channels, only those bits are used.