:STATus:CLIPped:ALL:CONNection:EVENt?

Query Syntax

:STATus:CLIPped:ALL:CONNectionN:EVENt?

Description

Reads the Clipped All Connection register to see which banks of channels have reported ADC clipping since the last time the register was read.

Reading the register once will clear the status for all instruments.

Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically "OR"ed, which results in setting true bit N-1 (CONNN) of the Clipped All Register.

Clipped All Register Commands
Register Read Write Command
Event ♦   :STATus:CLIPped:ALL:CONNection:EVENt?
Enable (mask) ♦ ♦ :STATus:CLIPped:ALL:CONNection:ENABle
Clipped All Register Bits
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32768 16384 8192 4096 2048 1024 512 256 128 64 32 16 8 4 2 1
Event
Register
— — — — — — — — — — — — — — — BANK1
Enable
Register
                               
Sets to Bit N-1 (CONNN) of Clipped All Register

Bit Definitions

BANK1
A true indicates the channels on bank 1 reported ADC clipping since the last time the register was read.