Distributed VNA Measurement (S9x571B)

Overview

This S9x571B application allows you to configure two VNA sets (PXI or Streamline) separated by up to 5 meters. This capability enables long‑distance S‑parameter measurements, such as cable testing and antenna characterization, while providing improved dynamic range and measurement stability.

 

Supported Model

S9x551B Multiple instruments/modules measurements is also required.

Configuration

The Distributed VNA requires one reciprocal thru cable to make the Auto refresh Cal. The thru cable must be connected during measurements.

The DUTs can be connected on the other ports. The figure shows an example of Streamline VNA.configuration. If phase measurement is not required, The thru cable for Auto Refresh Cal is not necessary.
 

When your DUT is a thru cable, the cable for auto refresh calibration (ports 1 to 6 in this example) can be a DUT. In that case, the path for auto refresh cal must be connected during the measurements. Otherwise, "Auto Refresh cal is inactive" will be displayed.

Configuration for Streamline

Two units of Strealeamline VNA can be configured as shown in the figure above. 

The required accessories are: 

Configuration for PXI 

The limitation of PXI configuration are:

 

The following two configurations are supported.

Please refer to configuration guide for the required components.

The following figure shows the configuration using PCIe Cable connection with an external host PC.

 

Measurement Procedure

  1. Power on the two modules or chassis after configuration is completed (LO cables and control cables must be connected before power on)

  2. Launch the VNA application

  3. Activate the Distributed VNA.

  4. Select the measurement class and setup your desired measurement setting.

  5. Execute the calibration

  6. Turn on Auto Refresh

  7. Execute the DUT measurements

Activate Distributed VNA

 

To activate the distributed VNA feature

  1. Click Setup > Internal Hardware > Distributed VNA, then Distributed VNA dialog box is displayed

  2. Check Enable distributed VNA, then click OK.

  3. Preset is done.

  4. DistVNA is displayed in the status bar.

Setup the measurement setting 

 

Set up your desired settings. Auto Refresh Cal has the following limitations. If phase measurement is not required, ignore this limitation because Auto Refresh Cal is unnecessary.  

 

Reciprocal Thru Cable Insertion Loss

If the reciprocal thru is too lossy, measurement errors increase and Auto Refresh Cal may not function correctly. To minimize measurement errors, the following conditions are recommended:

For M980xA, P500xB, P502xB, and P502xM (x = 5–8), meet these conditions from 500 kHz to 50 GHz.


If the reciprocal thru is too lossy, the following warning is displayed and no correction is applied. This warning also is displayed when a reciprocal thru cable is not connected.

"Auto Refresh Cal is inactive. Path Px-x is too lossy."

When using a reciprocal thru cable with loss exceeding 20 dB, this warning may appear but you can disable it by clearing the Check Path checkbox. However, do so with caution and compensate by tightening other measurement condition, such as increasing Output Power above −5 dBm, reducing IFBW below 100 kHz, and enabling Averaging (or increasing the averaging factor). For example, if the reciprocal thru loss is 30 dB (20 dB limit + 10 dB), increase Output Power by 10 dB to +5 dBm, or reduce IFBW by a factor of 10 Hz to 10 kHz, or increase the averaging count by a factor of 10 to 10 averages.


Frequency Range


For M980xA, P500xB, P502xB, and P502xM (x = 5-8), measurement errors are large below 500 kHz and above 50 GHz. In these ranges, Auto Refresh Cal uses measurement values from other frequencies to perform the correction. Therefore, correction cannot be applied if the measurement range is entirely below 500 kHz or entirely above 50 GHz, because no usable in-range frequency points are available for the correction. Set Frequency Start to 50 GHz or below and Frequency Stop to 500 kHz or above. If these conditions are not met, the following warning is displayed and no correction is applied:
"Auto Refresh Cal is inactive. Frequency Range cannot be corrected."

 

Number of Points


If the calibration is executed while at a distance for two units, Number of Point should meet the criteria

Execute Calibration

 

If two VNA sets can be placed closely during the calibration, the calibration steps can be reduced. Hence, there are two cases for calibration.

Case 1: Two VNA sets placed (PXI or Streamline) separated.

The calibration step is as shown below. Confirm if the number of points meets the required condition before the calibration.

  1. Click Cal > Main > Smart Cal (or Cal > Main > Other Cals > ECal... for ECal)

  2. Select the required calibration ports and options. Then,

  3. Define the Connector, DUT gender and Cal Kit. Check the "Modify Cal Type". Then, click Next for the next dialog.

  4. Define the 1st port and 2nd port for each thru. 

    1. Assign one port as a key 1st Port in the module (or Chassis) No.1.  In the example below, port 1.

    2. Assign each other ports in module No. 1 as 2nd port as "ECal Thru as Unknow thru" for Ecal, or "Unknown Thru" for mechanical cal kits. 

      • Thru #1: 1-2

      • Thru #2: 1-3

      • Thru #3: 1-4

    3. Assign one port in the module No.1 and one port in the module No.2 as Unknown Thru.

      • Thru #4: 1-6 

    4. Assign one port as a key 1st port in the module (or chassis) No.2. In the example below, port 5

    5. Assign each other ports in module No. 2 as 2nd port as "ECal Thru as Unknown thru" for Ecal, or "Unknown Thru" for mechanical cal kits. 

      • Thru#5: 5-6

      • Thru#6: 5-7

      • Thru#7: 5-8

    6. Click Next for the next dialog.

  5.   Follow the instruction to execute the calibration.

Note: During the Thru measurement in step 4c (Thru #4: 1-6), do not move the long LO cable connecting the two modules.

Note: When using the ECal, a long USB cable is required to reach the remotely located VNA. A powered USB hub is also necessary to provide sufficient power to the ECal. Connect a long USB cable to the PC, with a powered USB hub at the other end, to which the ECal is connected. 

 

 Example 1: Streamline 8 port configuration. Ports 1 to 4 in the module No.1, ports 5 to 8 in the module No.2

 

 

Example 2: PXI 20 port configuration , Ports 1 to 10 in the chassis No.1, Ports 11 to 20 in the chassis No.2   

 

1st Port

2nd Port 

Thru Cal Method for Ecal

Thru Cal Method for mechanical cal kits

Thru #1

1

2

ECal Thru As Unknown Thru

Unknown Thru

Thru #2

1

3

ECal Thru As Unknown Thru

Unknown Thru

Thru #3

1

4

ECal Thru As Unknown Thru

Unknown Thru

Thru #4

1

5

ECal Thru As Unknown Thru

Unknown Thru

Thru #5

1

6

ECal Thru As Unknown Thru

Unknown Thru

Thru #6

1

7

ECal Thru As Unknown Thru

Unknown Thru

Thru #7

1

8

ECal Thru As Unknown Thru

Unknown Thru

Thru #8

1

9

ECal Thru As Unknown Thru

Unknown Thru

Thru #9

1

10

ECal Thru As Unknown Thru

Unknown Thru

Thru #10

1

11

Unknown Thru

Unknown Thru

Thru #11

11

12

ECal Thru As Unknown Thru

Unknown Thru

Thru #12

11

13

ECal Thru As Unknown Thru

Unknown Thru

Thru #13

11

14

ECal Thru As Unknown Thru

Unknown Thru

Thru #14

11

15

ECal Thru As Unknown Thru

Unknown Thru

Thru #15

11

16

ECal Thru As Unknown Thru

Unknown Thru

Thru #16

11

17

ECal Thru As Unknown Thru

Unknown Thru

Thru #17

11

18

ECal Thru As Unknown Thru

Unknown Thru

Thru #18

11

19

ECal Thru As Unknown Thru

Unknown Thru

Thru #19

11

20

ECal Thru As Unknown Thru

Unknown Thru

     

Required Number of Point

 

As this calibration uses a long thru cable, the unknown thru calibration requires larger number of points to determine the cable length.

 

Example Calculation

Step 1: Calculate the maximum Δf

Δf < (0.66 × 2.997925E8 ) / (4×5)

Δf < 9.8 MHz
 

Step 2: Calculate the minimum number of points
number of points > (50  GHz / 9.8  MHz)+1

number of points >= 5103

Thus, at least 5103 points are required for the analyzer to automatically determine the Thru cable delay.

 

Reference for maximum Δf calculation

The maximum allowable frequency step (Δf) for automatic Thru cable delay estimation is determined using the following formula:


   Δf<(V_f × c) / (2×l)

 

Where:
    l = physical length of the Thru cable (meters)
    Δf = frequency step size = span / (points − 1)
    Vf = velocity factor of the Thru cable
    c = speed of light = 2.997925 × 10⁸ m/s


A smaller Δf (i.e., more measurement points) enables the instrument to accurately determine the electrical delay of the Thru cable.

Case 2: Two VNA sets can be moved closely during calibration 

If the two VNA sets can be moved at the same place during calibration, there are the following benefits.

The calibration steps are the same as Case 1, with the following difference:

When assigning the cross-module thru (Thru #4: 1-6), select "ECal Thru as Unknown Thru" for ECal, or "Unknown Thru" for mechanical cal kits — the same as all other thru assignments.

Note: During the Thru measurement in step 4c (Thru #4: 1-6), do not move the long LO cable connecting the two modules. 

 

Example 1: Streamline 8 port configuration. Ports 1 to 4 in the module No.1, ports 5 to 8 in the module No.2

 

1st Port

2nd Port 

Thru Cal Method for Ecal

Thru Cal Method for mechanical cal kits

Thru #1

1

2

ECal Thru As Unknown Thru

Unknown Thru

Thru #2

1

3

ECal Thru As Unknown Thru

Unknown Thru

Thru #3

1

4

ECal Thru As Unknown Thru

Unknown Thru

Thru #4

1

 6

ECal Thru As Unknown Thru

Unknown Thru

Thru #5

 5

6

ECal Thru As Unknown Thru

Unknown Thru

Thru #6

 5

7

ECal Thru As Unknown Thru

Unknown Thru

Thru #7

5

8

ECal Thru As Unknown Thru

Unknown Thru

 

Example 2: PXI 20 port configuration , Ports 1 to 10 in the chassis No.1, Ports 11 to 20 in the chassis No.2   

 

1st Port

2nd Port 

Thru Cal Method for Ecal

Thru Cal Method for mechanical cal kits

Thru #1

1

2

ECal Thru As Unknown Thru

Unknown Thru

Thru #2

1

3

ECal Thru As Unknown Thru

Unknown Thru

Thru #3

1

4

ECal Thru As Unknown Thru

Unknown Thru

Thru #4

1

5

ECal Thru As Unknown Thru

Unknown Thru

Thru #5

1

6

ECal Thru As Unknown Thru

Unknown Thru

Thru #6

1

7

ECal Thru As Unknown Thru

Unknown Thru

Thru #7

1

8

ECal Thru As Unknown Thru

Unknown Thru

Thru #8

1

9

ECal Thru As Unknown Thru

Unknown Thru

Thru #9

1

10

ECal Thru As Unknown Thru

Unknown Thru

Thru #10

1

11

ECal Thru As Unknown Thru

Unknown Thru

Thru #11

11

12

ECal Thru As Unknown Thru

Unknown Thru

Thru #12

11

13

ECal Thru As Unknown Thru

Unknown Thru

Thru #13

11

14

ECal Thru As Unknown Thru

Unknown Thru

Thru #14

11

15

ECal Thru As Unknown Thru

Unknown Thru

Thru #15

11

16

ECal Thru As Unknown Thru

Unknown Thru

Thru #16

11

17

ECal Thru As Unknown Thru

Unknown Thru

Thru #17

11

18

ECal Thru As Unknown Thru

Unknown Thru

Thru #18

11

19

ECal Thru As Unknown Thru

Unknown Thru

Thru #19

11

20

ECal Thru As Unknown Thru

Unknown Thru

     

 

Activate Auto Refresh Cal

Auto Refresh Cal compensates the phase drift of local signal due to a cable movement and temperature change. 

  1. Click Cal > Other Cals > Auto Refresh Cal...

  2. Select the thru path for auto refresh cal.

  3. Check Enable Auto Refresh, then click OK.

  4. Disable if Check Path function is not required.

  5. ARefresh is displayed in the status bar.

Execute the DUT measurements

Limitation

 

Supported Application and Feature

Model

Description

Supported 

S9x007A/B

Automatic Fixture Removal

Yes

S9x008B

Probe and Fixture Leakage Calibration

No

S9x010A/B

Time Domain

Yes

S9x011B

Enhanced time domain analysis with TDR

Yes (Advance Mode)

See the limitation for TDR

S9x015B

Real-time S-Parameter and Power Measurement Uncertainty

No

S9x024B

Basic Pulsed-RF Measurements, Lite

No

S9x025A/B

Basic Pulsed-RF Measurements

No

S9x027B

Mechanical noise tuner control

No

S9x029A/B

Noise Figure Measurements with Vector Correction

No

S9x050B

IQ data bandwidth up to 1.5 GHz

No

S9x051B

IQ data bandwidth up to 4 GHz

No

S9x070B

Modulation distortion

No

S9x082A/B

Scalar Mixer Converter (SMC) measurements

No

S9x083A/B

Vector & Scalar Mixer/Converter Measurements

No

S9x084A/B

Embedded LO Capability

No

S9x086A/B

Gain-Compression Measurements

No

S9x087B

Swept IMD for Amplifiers

No

S9x088B

Source Phase Control

No

S9x089B

Differential and I/Q device measurements

No

S9x090A/B

Spectrum Analysis

No

S9x111B

Active Hot Parameters

No

S9x460B

True-Mode Stimulus

No

S9x551A/B

Multiple Instruments/modules measurements

Required

S9x552B

Multiport calibration assistant / Multiport ECal for PXI Switches

No

S9x553B

Multiport calibrated measurements with switch instruments

No

S9x560B

N5252AWxx

No

 

The following features are not supported.

Limitation for TDR