:ACQuire:ECOunt
Instrument:
N1010A
N1000A
DCA-M
UXR Scope
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:ACQuire:ECOunt <count>
<count> is an int.
Query Syntax
:ACQuire:ECOunt?
Description
Sets the number of waveforms to use in the smoothing calculation with smoothing is enabled (:ACQuire:SMOothing). You can enter a value between 2 and 32,768. The default value for the number of averages is 16. For some types of waveforms, it may take some time to reach the number of waveforms specified. In this case, use the :MEASure:ACQuire:ECOUNT? query to return the current count number.
Common Numerical Child Commands
This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.