:ACQuire:SPERiod:MODE
Instrument:
N1000A
Meas. mode:
TDR
Flex Apps:
FlexDCA
Command Syntax
:ACQuire:SPERiod {AUTomatic | MANual}
Query Syntax
:ACQuire:SPERiod?
Description
This TDR mode command selects between AUTomatic or MANual entry of Sample Period (record length). For additional information, refer to TDR waveform acquisition and display.
- AUTomatic
- FlexDCA automatically sets the record length to optimize the sample period. Automatic is the default setting.
- MANual
- Allows you to set the sample period using the
ACQuire:SPERiodcommand.
This command requires TDR Mode with an active TDR step (calibrated) displayed.
Requires FlexDCA revision A.07.80 and above.
Example Command Sequence
:ACQuire:RSPec SPERiod :ACQuire:SPERiod:MODE MANual :ACQuire:SPERiod 15.625e-15 :DISK:WAVeform:SAVE:FTYPe WYValues :DISK:WAVeform:EOSPoints ON :DISK:WAVeform:SAVE