:ACQuire:RLENgth:MODe
Instrument:
N1010A
N1000A
DCA-M
UXR Scope
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:ACQuire:RLENgth:MODe {AUTomatic | MANual}
Query Syntax
:ACQuire:RLENgth:MODe?
Description
Select between AUTomatic or MANual entry of Samples / Waveform (record length). The record length is the number of waveform samples acquired across a single sweep. Changing the samples / waveform affects sweep time (display update rate), histograms, and measurements.
- AUTomatic
- FlexDCA sets the record length to optimize the single record length versus total database update rate. This is the default setting and is recommended when color grade or gray scale waveform persistence, or a histogram, or a mask test is enabled. In Jitter Mode, the record length is set to
AUTomaticand cannot be changed. - MANual
- Allows you to specify the samples / waveform from as few as 16 points using the
ACQuire:RLENgthcommand. The default value is 2048 points.
The record length definition is locked to samples / UI this command is unavailable, if both pattern locking (:TRIGger:PLOCk) and acquire entire pattern (:ACQuire:EPATtern) is turned on.
Requires FlexDCA revision A.01.80 and above.
Example Command Sequence
:ACQuire:EPATtern OFF :ACQuire:RSPec RLENgth :ACQuire:RLENgth:MODe MANual :ACQuire:RLENgth 4096