:ACQuire:RSPec
Instrument:
N1010A
DCA-X
DCA-M
UXR Scope
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:ACQuire:RSPec {RLENgth | SPUI | SPERiod}
Query Syntax
:ACQuire:RSPec?
Description
Selects the waveform record length to be based on Samples / Waveform, Samples / UI (Unit Interval), or Sample Period. For additional information, refer to TDR waveform acquisition and display.
- RLENgth
- Defines the record length as Samples / Waveform. Use the
:ACQuire:RLENgth:MODEcommand to select automatic or manual mode. In manual mode, useACQuire:RLENgthto enter the number of points. In Jitter Mode, the record length is set to Samples / Waveform and cannot be changed. - SPERiod
- Defines the record length as Sample Period. Use the
:ACQuire:SPERiod:MODEcommand to select automatic or manual mode. In manual mode, useACQuire:SPERiodto enter the sample period. This is a TDR Mode only command that is only available when an active TDR step (calibrated) is displayed. This argument was introduced in FlexDCA revision A.07.80 and above. - SPUI
- Defines the record length as Samples / UI. Use the
:ACQuire:SPUI:MODEcommand to select automatic or manual mode. In manual mode, useACQuire:SPUIto enter the number of points. This argument applies to FlexDCA revision A.05.60 and above. - SPBit (deprecated)
- Defines the record length as samples-per-bit. Use
:ACQuire:SPBit:MODEto set automatic or manual mode and, if manual is selected, useACQuire:SPBitto enter the number of samples. When writing new programs, use theSPUIargument instead.
The record length definition is locked to samples-per-UI, if both pattern locking (:TRIGger:PLOCk) and acquire entire pattern (:ACQuire:EPATtern) is turned on.
Example Command Sequence
For Scope and Eye modes
:ACQuire:EPATtern OFF :ACQuire:RSPec RLENgth :ACQuire:RLENgth:AUTo MANual :ACQuire:RLENgth 4096
For TDR mode
:ACQuire:RSPec SPERiod :ACQuire:SPERiod:MODE MANual :ACQuire:SPERiod 15.625e-15 :DISK:WAVeform:SAVE:FTYPe WYValues :DISK:WAVeform:EOSPoints ON :DISK:WAVeform:SAVE