:ACQuire:REYE:ALIGn

Instrument:
N1000A
N107x-JSA
N1060A-JSA
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
L-SNT
Waveforms:
NRZ
PAM4

Command Syntax

:ACQuire:REYE:ALIGn {ON | OFF | 1 | 0}

Query Syntax

:ACQuire:REYE:ALIGn?

Query Response

{1 | 0}

Description

If multiple eye diagrams are displayed, configures an Auto Scale (:SYSTem:AUToscale) to align the eyes when rapid eye is on (:ACQuire:REYE). The eye diagrams are aligned using software delay.

Rapid Eye requires FlexDca be placed in Eye/Mask mode without pattern locking.

Parent Command