:ACQuire:SINGle
Instrument:
N1010A
N1000A
DCA-M
UXR Scope
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:ACQuire:SINGle
Description
If the acquisition is in Run mode, the current acquisition sweep is completed and the acquisition is stopped after the last data point is acquired. If the acquisition is in Stop mode, a single waveform acquisition is performed. All measurements are performed when the acquisition is updated. This command does not erase display memory. To clear display memory, use the :ACQuire:CDISplay command.
Some situations may require the use of an *OPC? query with this command to pause program execution.
For FlexPLL application, requires revision A.06.70 and above.