:ACQuire:REYE:INTerval
Instrument:
N1000A
N107x-JSA
N1060A-JSA
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND
L-SNT
Waveforms:
NRZ
PAM4
Command Syntax
:ACQuire:REYE:INTerval <unit_intervals>
<unit_intervals> is an int.
Query Syntax
:ACQuire:REYE:INTerval?
Description
Specifies the number of UI (Unit Intervals) to acquire the data from for Rapid Eye. The database is expanded as required for the number of UIs, while keeping the displayed eye (usually 1.6 UIs) unchanged. Use the :ACQuire:REYE command to turn on Rapid Eye measurements.