:DISK:DWIZard:TPERcent{1:4}:SDATa
Command:
Deprecated
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.05.40 and above, use the :DISK:DWIZard:T:PERCent:SDATa command instead.
Command Syntax
:DISK:DWIZard:TPERcent{1:4}:SDATa {ON | OFF}
Description
When a Documentation Wizard zip file is saved (:DWIZard:SAVE), use this command to add a data file for each displayed T-parameter waveform in any Time-% waveform content windows. These are ASCII XY-value waveform files and one file is saved for each displayed waveform (for example, T21 Percent.txt). A screen capture of the Time-% waveform content window is also saved (Time-% N Window Screen Capture.png). TDR mode (:SYSTem:MODE) must be selected.
| Argument | Action |
|---|---|
| ON | Includes files in Documentation Wizard zip file |
| OFF | Excludes files in Documentation Wizard zip file |
Query Syntax
:DISK:DWIZard:TPERcent:SDATa?
Query Response
{1 | 0}
Requires FlexDCA revision A.04.50 and above.