:DISK:EYE:RECall
Command:
Deprecated
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.05.70 and above, use the :EMEMory:FILE:LOAD command instead.
Command Syntax
:DISK:EYE:RECall
Description
Loads a color grade-gray scale file into one of eight waveform memory locations or into jitter memory as specified by the :DISK:EYE:RECall:DESTination command to select the waveform memory. Use the :DISK:EYE:FNAMe command to specify the file to load.