:DISK:EYE:RECall:DESTination
Command:
Deprecated
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.05.70 and above, use the :EMEMory:FILE:LOAD command instead.
Command Syntax
:DISK:EYE:RECall:DESTination {CGMemory1 | CGMemory2 | CGMemory3 | CGMemory4 | CGMemory5 | CGMemory6 | CGMemory7 | CGMemory8}
Query Syntax
:DISK:EYE:RECall:DESTination?
Description
In Eye/Mask, selects one of eight eye memory locations to load a color grade-gray scale file. Use the :DISK:EYE:RECall parent command to actually load the file into the indicated memory.