:FEYE:DIFF:SID
Command Syntax
:FEYE:DIFF{1:8}{A|C}:SID SESSion{1:16}
Where {1:8}{A|C} identifies the differential waveform by module slot and input channel. For example, the differential waveform of channels 1A and 2A would be identified as :DIFF1A.
Query Syntax
:FEYE:DIFF{1:8}{A|C}:SID?
Query Response
SESS{1:8}
Description
Assigns a FlexEye session identifier number to the specified differential channel. Station numbers can be any integer from 1 through 16. The session number represents one instance of an independent FlexDCA sampling oscilloscope. The session's VISA address is derived from the session number.The same session number can be assigned to multiple channels (single-ended or differential). In the case of a differential signal (two electrical channels), both channels must be assigned the same session number. Station number assignments can also be viewed in the FlexEye Acquisition dialog. To turn on the FlexEye, use the :FEYE:STATe command. The query form of the command returns the session ID number.
Requires FlexDCA revision A.05.40 and above.
Example Command
:FEYE:DIFF1A:SID SESSion4