:FEYE:SPUI

Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
NRZ
PAM4

Command Syntax

:FEYE:SPUI <double>

Where <double> is the number of samples-per-UI. For example, 4.096E+03.

Query Syntax

:FEYE:SPUI?

Description

Sets the number of samples acquired per unit interval (UI) during data acquisition in a FlexEye session. The minimum value is 1 samples/UI. The maximum value is 4096 samples/UI. This command is equivalent to the Samples / UI setting in the FlexEye Streaming Setup dialog.

Requires FlexDCA revision A.05.80 and above.

Example Command

:FEYE:SPUI 1.099212598E+1