:FEYE Subsystem
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
NRZ
PAM4
Use the commands in this subsystem to configure FlexEye Independent Eye Acquisition and Analysis. With these commands you can select the channels, assign the session identifier, and turn FlexEye on. FlexEye can only be used with the HiSLIP VISA interface. FlexEye is not compatible with VXI-11, Telnet, Sockets, or GPIB.
Click the following links to learn about example Python programs :
- Python Example of configuring a variety of FlexEye sessions (simulated modules)
- Python Example of child process that communicates with the parent via stdout (simulated modules)
- Python Example of child process with tkinter graph (simulated modules)
This subsystem requires FlexDCA revision A.05.40 and above.