:FEYE:SAMPles
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
NRZ
PAM4
Command Syntax
:FEYE:SAMPles <count>
<count> is an int.
Query Syntax
:FEYE:SAMPles?
Description
Sets the number of Samples per Eye. The time spacing between measurement points can affect interpolation between the points used to make measurements. Increasing the sample number increases the time required to capture a single sweep. The default value is 1024 points. This command is similar to the :ACQuire:RLENgth command which sets the number of sample points for normal acquisition without FlexEye running.
Requires FlexDCA revision A.05.40 and above.
Example Command
:FEYE:SAMPles 2047