:FEYE:CHANnel:SID

Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
NRZ
PAM4

Command Syntax

:FEYE:CHANnel{1:8}{A|B|C|D}:SID SESSion{1:16}

Where the specifier {1:8}{A|B|C|D} identifies a specific channel. For example, CHANnel3C.

Where the {1:15} specifies a station number.

Query Syntax

:FEYE:CHANnel{1:8}{A|B|C|D}:SID?

Description

Assigns a FlexEye session identifier number to the specified channel. Station numbers can be any integer from 1 through 16. The session number represents one instance of an independent FlexDCA sampling oscilloscope. The session's VISA address is derived from the session number. The same session number can be assigned to multiple channels (single-ended or differential). Station number assignments can also be viewed in the FlexEye Acquisition dialog. To turn on the FlexEye, use the :FEYE:STATe command. The query form of the command returns the session ID number.

Requires FlexDCA revision A.05.40 and above.

Example Command

:FEYE:CHANnel2C:SID SESSion3