:FEYE:STATe
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
NRZ
PAM4
Command Syntax
:FEYE:STATe {PAUSe | RUN | STOP}
Query Syntax
:FEYE:STATe?
Description
Controls the state of Independent Eye Acquisition.
PAUSe- Halts FlexEye from streaming data. FlexEye is also set to
PAUSemode if you send a:SYSTem:GTLocalcommand to place FlexDCA in local mode. With FlexEye paused you can make changes to FlexEye session configuration or change FlexDCA settings. RUN- Runs FlexEye with each Station running as an independent sampling oscilloscope.
STOP- Exits FlexEye mode restoring FlexDCA to its standard GUI without FlexEye tabs.
Use an *OPC? query to pause program execution while waiting for this command to execute.
Requires FlexDCA revision A.05.40 and above.
Example Command
:FEYE:STATe PAUSe