:FEYE:UPLock
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
NRZ
PAM4
Command Syntax
:FEYE:UPLock {ON | OFF | 1 | 0}
Query Syntax
:FEYE:UPLock?
Query Response
{ON | OFF | 1 | 0}
Description
Turns on and off the use of pattern locking in the FlexEye application. This is equivalent to selecting the Use Pattern Lock setting in the FlexEye Streaming Setup dialog.
Requires FlexDCA revision A.05.80 and above.
Example Command
:FEYE:UPLock ON