:FEYE:CHANnel:ENABled
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
NRZ
PAM4
Command Syntax
:FEYE:CHANnel{1:8}{A|B|C|D}:ENABled {ON | OFF}
Where the specifier {1:8}{A|B|C|D} identifies a specific channel. For example, CHANnel3C.
Query Syntax
:FEYE:CHANnel{1:8}{A|B|C|D}:ENABled?
Description
Selects a channel to be used for FlexEye. To assign the session number for the selected channel, use the :FEYE:CHANnel:SID command. To turn on FlexEye independent eye acquisition and analysis, use the :FEYE:STATe command.
Requires FlexDCA revision A.05.40 and above.
Example Command
:FEYE:CHANnel2C:ENABled ON