:FEYE:CHANnel:SIRC
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
NRZ
PAM4
Command Syntax
:FEYE:CHANnel{1:8}{A|B|C|D}:SIRC {ON | OFF}
Where the specifier {1:8}{A|B|C|D} identifies a specific channel. For example, CHANnel3C.
Query Syntax
:FEYE:CHANnel{1:8}{A|B|C|D}:SIRC?
Description
Turns the use of SIRC (System Impulse Response Correction) data on or off on the selected channel for N1092-series modules. To enable the channel for Flexeye, use the :FEYE:CHANnel:ENABled command. To turn on FlexEye independent eye acquisition and analysis, use the :FEYE:STATe command.
SIRC data, installed on N1092-series modules, can be used with FlexEye. SIRC data on other modules is not compatible with FlexEye.
Requires FlexDCA revision A.05.70 and above.
Example Command
:FEYE:CHANnel2C:SIRC ON