:REPository:MEASure:CRECovery:SELection:ALL
Command Syntax
:REPository:MEASure:CRECoveryN:SELection:ALL
Where N identifies the slot number and must be selected from {1:8}. The slot number is associated with the N1076A, N1077A, or 86108A/B Precision Waveform Analyzer module with Option JSA. When an 86108A/B module is used, the slot number is always 1.
Description
For the Selected publishing mode, selects to publish all JSA Results panel measurements. Use the :REPository:MEASure:AMPLitude:SELection:CLEar
sibling command to exclude all JSA Results measurements. Use the :REPository:MEASure:AMPLitude:SELection
parent command to select specific JSA Results measurements or the query form to return the currently selected measurements.
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.