:REPository:MEASure:JITTer:SELection:ALL
Meas. mode:
Jitter
Waveforms:
NRZ
Publish mode:
Selected
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:REPository:MEASure:JITTer:SELection:ALL
Description
For the Selected publishing mode, selects to publish all Jitter Mode jitter measurements in the Jitter panel. Use the :REPository:MEASure:JITTer:SELection:CLEar
sibling command to exclude all Jitter Mode Jitter measurements. Use the :REPository:MEASure:JITTer:SELection
parent command to select specific Jitter measurements or the query form to return the currently selected measurements.
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.