:REPository:MEASure:JITTer:SELection
Command Syntax
:REPository:MEASure:JITTer:SELection <measurements>
Where <measurements> is a comma-separated string that selects one or more measurements. For example, "1,3,5".
Query Syntax
:REPository:MEASure:JITTer:SELection?
Description
For the Selected publishing mode, selects to publish one or more Jitter Mode's measurements that are listed in the Jitter panel. Measurements are identified using an index that represents the measurement's location in the panel. In this picture, the index for TJ is 1, DJ is 2, and RJ is 3. Programmatically, the you can return the index using the measurement's child :LOCation?
query.
Example Command Sequence
To return the location of the DJ measurement, you would use these commands.
FlexDCA.write(':REPository:MEASure:PMODe SELected') index = FlexDCA.query(':MEASure:JITTer:DJ:LOCation?') FlexDCA.write(':REPository:MEASure:JITTer:SELection ' + index)
Indexes
- To find a measurement's index by query
- To find a measurement's index from FlexDCA's GUI
- More information on measurement indexes
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.