:REPository:MEASure:HISTogram:SELection:CLEar
Meas. mode:
Scope
Eye
TDR
Publish mode:
Selected
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:REPository:MEASure:HISTogramN:SELection:CLEar
Where N identifies one of four possible histograms {1:4} that you can design. For example, :HISTogram3
.
Description
For the Selected publishing mode, excludes all histogram measurements in the Histogram panel from being published. Use the :REPository:MEASure:HISTogram:SELection:ALL
sibling command to include all Histogram panel measurements. Use the :REPository:MEASure:HISTogram:SELection
parent command to select specific Histogram panel measurements or the query form to return the currently selected measurements.
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.